AXIS#.IL.IFOLD

Description

Two current foldback algorithms run in parallel in the drive: the drive foldback algorithm and the motor foldback algorithm. Each algorithm uses different sets of parameters.

Each algorithm has its own foldback current limit, AXIS#.ILClosed"Instruction list" This is a low-level language and resembles assembly.DIFOLD and AXIS#.IL.MIFOLD. The overall foldback current limit at any moment is:

AXIS#.IL.IFOLD = min (AXIS#.IL.DIFOLD, AXIS#.IL.MIFOLD, AXIS#.IPEAK)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

A

Range

0 to 2,147,483.647 A

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.IFOLD 0x500A 0xC DINT 1000:1 - RO False
AXIS2.IL.IFOLD 0x510A 0xC DINT 1000:1 - RO False